Low Cost Automation
Automotive companies face many challenges in their production lines like testing, inspection, precision and so on. We came across one such situation where an automobile engine manufacturer was facing a problem in their engine valve inspection line. The problem was that each of the valve guide pins should be positioned precisely to get the exact […]
Igus Low cost Automation (LCA) has a full fledged customer testing area. This helps customer to simulate his application and ensure that it works with igus solution before placing the order. This helps a lot of customers also with faster turnaround of their automation projects, which leads to faster Return on Investment (ROI). With igus […]
how the application range of a cobot can be expanded with the use of drylin® ZLW, the so-called “7th axis”,is shown by the company RHEWUM® based in Remscheid. The company uses components and systems from Low Cost Automation when welding components with a collaborative robot. The use of low cost automation components helps the company to automate production cost-effectively. Reading […]
Although robotics and automation have many advantages for employees, production processes and customers, they are still viewed critically, especially by SMEs. Breaking into automation, especially for those with little affinity for IT, often involves high investment and great effort. But robot manufacturers are increasingly focusing on cost-effective alternatives that are as user-friendly and as easy […]
igus® gantries are used in countless different applications and industries, from picking & placment of components to pipetting applications. The opportunities are endless when it comes to igus® gantries, whether an application requires a speed of upto 1 m/s, accuracy of +/-0.5 mm with loads up to 10 kgs, the solution will be found using […]
In the last couple of years, we have faced through various challenges mainly due to the COVID-19 pandemic. The key issue everyone witnessed was the sustained fluctuation of demands along with a lack of trained labour. The below application story shows the instance of one of our customers where his problem was countered using igus […]
Automation of the manufacturing process is a critical need for the current industry to stay competitive and improve quality and reliability. This also allows better use of human resources. With the pandemic and shortage for manpower in the current scenario we are also pushed by circumstances. Most of the repetitive, mundane tasks could be automated. […]
Igus has introduced Stepper & DC Drives for controlling DC, BLDC & stepper motors. This article is particularly about the Stepper Drive, which is called igus D1 Drive. We offer this D1 (Stepper Drive) along with our screw-driven and belt-driven systems. The igus D1 Drive acts as a versatile single-axis motor controller, ensuring smooth stepper […]
igus has introduced 7th axis for Robots which is one on the NEWS product on 2020. The idea behind this development is that the existing robots can be moved up to 3 meters either in Vertical or Horizontal orientation – so one robot can handle two or three machines depending on the space available. Construction: […]
Especially now, preventive hygiene measures, or hygiene management, are in the spotlight. Especially in public facilities such as hotels, schools or hospitals, they play an indispensable role. Disinfection robots can provide a remedy here. But how safe is this new technology and is the use of robots worthwhile for public institutions? Time to take a […]