igus® was founded on October 15, 1964, in a garage in Cologne-Mülheim. Since then, we’ve been creating innovative, lubrication-free plastics that keep the world moving. Our products are used in cars, cranes, furniture, machines, robots, and even bicycles. One example is the igus®, a unique urban bike made from recycled plastic. It showcases many of […]
Our chainflex cables are versatile and can be used in many different applications. They work well indoors and outdoors, in hot and cold places, in cleanrooms, and in oily air. But how do these cables perform as cables in radioactive environments? What is Radiation? Radiation is the movement of particles or waves. They are subdivided […]
Anyone who’s worked with metallic insert bearings is likely aware of the frequent — and frankly tedious — relubrication efforts required for such components. Without the proper lubrication, these bearings are almost certain to wear prematurely and fail, leading to costly downtime and lost production. This may seem like an unavoidable reality, however there’s a […]
Several industrial applications require bearings with self-aligning features and this is generally achieved by using spherical bearings. A spherical plain bearing is a bearing that permits angular movement around a central point. igubal is a range of polymer spherical bearings from igus GmbH. Like all the other products from igus, igubal bearings offer many advantages over metal spherical bearings. Here are […]
At customers’ premises, I often observe how the electricians unwind cables from the cable reels or remove them from the cable ring in various ways during installation. You can go wrong here. Especially when the cable concerned is used for dynamic applications in energy chains, incorrect unreeling can have fatal consequences. To be honest, when I […]
“You don’t have to reinvent a wheel, just realign it.” This old quote holds true for a modern-day design engineer designing a machine. It is the reason why the designer likes to use off the shelf, standard “bought-out” parts wherever possible in his design. Fortunately, in today’s industry most of the established company has a […]
With the range of high performance, maintenance-free, lubrication-free, tribo-polymer plain bearings, igus can offer solution to heavy duty applications without need of greasing. These bearings offer high wear resistance at high loads. Heavy duty applications for plain bearings generally seen in construction machines, agricultural equipment, hydraulic cylinders, mounting brackets etc have very challenging technical requirements […]
Metallic plain bearings must be lubricated in order to function as a system. Grease is a part of the bearing system. On the other hand, with self-lubricating bearings like iglidur® plain bearings the addition of grease is not necessary. In the construction machinery industry, lubrication-free plain bearings have seen increasing use. Eliminating the need for […]