igus:bike World Tour

Shery George | 21 November 2024

igus® was founded on October 15, 1964, in a garage in Cologne-Mülheim. Since then, we’ve been creating innovative, lubrication-free plastics that keep the world moving. Our products are used in cars, cranes, furniture, machines, robots, and even bicycles. One example is the igus®, a unique urban bike made from recycled plastic. It showcases many of […]

Read more...

Cables in Radioactive Environments

Shery George | 12 June 2024

Our chainflex cables are versatile and can be used in many different applications. They work well indoors and outdoors, in hot and cold places, in cleanrooms, and in oily air. But how do these cables perform as cables in radioactive environments? What is Radiation? Radiation is the movement of particles or waves. They are subdivided […]

Read more...

Why should you chooseplastic insert bearings overmetal?

Shery George | 28 May 2024

Anyone who’s worked with metallic insert bearings is likely aware of the frequent — and frankly tedious — relubrication efforts required for such components. Without the proper lubrication, these bearings are almost certain to wear prematurely and fail, leading to costly downtime and lost production. This may seem like an unavoidable reality, however there’s a […]

Read more...

What is igubal and what benefits do they offer in the Automotive Industry?

Shery George | 17 August 2022

Several industrial applications require bearings with self-aligning features and this is generally achieved by using spherical bearings. A spherical plain bearing is a bearing that permits angular movement around a central point. igubal is a range of polymer spherical bearings from igus GmbH. Like all the other products from igus, igubal bearings offer many advantages over metal spherical bearings. Here are […]

Read more...

Latest news

Light & Quick Readychain Systems for Single Girder E.O.T. Cranes

Shery George | 8 December 2021

In modern crane technology Single Girder EOT Cranes are extensively used in warehouses, workshops, pre-cast manufacturing, sheet metal industry, automotive industries etc. Subsequently we also find applications in explosive, combustible, and corrosive environments as well. While majority of the single girder cranes fall into low duty cycles as the lifting capacities are also on the […]

Read more...

Maintenance free high performance igus polymer bearings for the pharmaceutical packaging industry

Shery George | 22 November 2021

With the changing times, the Indian Pharma industry is witnessing  dynamic changes & are adopting advanced technologies for their machines , manufacturing processes , packaging techniques and other related aspects , so  as to achieve greater output  & higher productivity without any compromise on the strict hygiene standards & to maintain the safety of the […]

Read more...

What are plain bearings and what advantages igus offers in Automotive industry?

Shery George | 12 November 2021

Plain bearings or commonly known as “bush”, bush bearing”, “bushing”, slide bearing” etc. are a much older technology when compared with ball bearings. Humans have been using plain bearings since year 3000BC. These are the simplest form of bearings without any rolling elements. Some of the most desired features of a plain bearings are – […]

Read more...

Selection of the Suitable mounting bracket

Shery George | 19 October 2021

Almost all mounting brackets are available in two variants. The first pivoting, the second is locking. At this point, many design engineers wonder when they should use the pivoting and when the locking version. Pivoting Type  Locking Type Pivoting mounting brackets are standard for gliding and horizontally unsupported applications: But why is that? The pivoting […]

Read more...