igus:bike World Tour

Shery George | 21 November 2024

igus® was founded on October 15, 1964, in a garage in Cologne-Mülheim. Since then, we’ve been creating innovative, lubrication-free plastics that keep the world moving. Our products are used in cars, cranes, furniture, machines, robots, and even bicycles. One example is the igus®, a unique urban bike made from recycled plastic. It showcases many of […]

Read more...

Cables in Radioactive Environments

Shery George | 12 June 2024

Our chainflex cables are versatile and can be used in many different applications. They work well indoors and outdoors, in hot and cold places, in cleanrooms, and in oily air. But how do these cables perform as cables in radioactive environments? What is Radiation? Radiation is the movement of particles or waves. They are subdivided […]

Read more...

Why should you chooseplastic insert bearings overmetal?

Shery George | 28 May 2024

Anyone who’s worked with metallic insert bearings is likely aware of the frequent — and frankly tedious — relubrication efforts required for such components. Without the proper lubrication, these bearings are almost certain to wear prematurely and fail, leading to costly downtime and lost production. This may seem like an unavoidable reality, however there’s a […]

Read more...

What is igubal and what benefits do they offer in the Automotive Industry?

Shery George | 17 August 2022

Several industrial applications require bearings with self-aligning features and this is generally achieved by using spherical bearings. A spherical plain bearing is a bearing that permits angular movement around a central point. igubal is a range of polymer spherical bearings from igus GmbH. Like all the other products from igus, igubal bearings offer many advantages over metal spherical bearings. Here are […]

Read more...

Latest news

Satisfying customer needs with igus Gantry Robot

Shery George | 11 February 2022

In the last couple of years, we have faced through various challenges mainly due to the COVID-19 pandemic. The key issue everyone witnessed was the sustained fluctuation of demands along with a lack of trained labour. The below application story shows the instance of one of our customers where his problem was countered using igus […]

Read more...

What do bend radius and minimum bend radius mean for cables?

Shery George | 1 February 2022

Time and again we talk about the bend radius in the field of energy chains and cables. We will take a closer look today what this means exactly and why the bend radius is so important. What is the bend radius? The bend radius is the radius in which a cable can be bent without […]

Read more...

Oil resistance for cables and cables

Shery George | 28 January 2022

Cables must always be selected according to the application and the external conditions. These include weather conditions, extreme or ambient temperature and also contact with oils. The oil resistance of cables is often indispensable. We shall clarify more background on the subject in today’s post. Why oil-resistant? Oils can damage plastics and also the materials of a […]

Read more...

xiros guide rollers with FDA conformity: 60% weight saving compared to metallic solutions

Shery George | 21 January 2022

igus, develops maintenance-free and above all lubrication-free solution for transport and guide rollers, which are made of blue light weight PVC tube and FDA-compliant two fixed flange ball bearings made up of in-house material xirodur B180 and stainless steel balls under the brand name xiros.  These xiros guide rollers  are particularly important for labelling, packaging and food applications due […]

Read more...