igus® was founded on October 15, 1964, in a garage in Cologne-Mülheim. Since then, we’ve been creating innovative, lubrication-free plastics that keep the world moving. Our products are used in cars, cranes, furniture, machines, robots, and even bicycles. One example is the igus®, a unique urban bike made from recycled plastic. It showcases many of […]
Our chainflex cables are versatile and can be used in many different applications. They work well indoors and outdoors, in hot and cold places, in cleanrooms, and in oily air. But how do these cables perform as cables in radioactive environments? What is Radiation? Radiation is the movement of particles or waves. They are subdivided […]
Anyone who’s worked with metallic insert bearings is likely aware of the frequent — and frankly tedious — relubrication efforts required for such components. Without the proper lubrication, these bearings are almost certain to wear prematurely and fail, leading to costly downtime and lost production. This may seem like an unavoidable reality, however there’s a […]
Several industrial applications require bearings with self-aligning features and this is generally achieved by using spherical bearings. A spherical plain bearing is a bearing that permits angular movement around a central point. igubal is a range of polymer spherical bearings from igus GmbH. Like all the other products from igus, igubal bearings offer many advantages over metal spherical bearings. Here are […]
Ached Backs and Strained necks are not a good combination for a long drive. A good comfortable driving position is derived from a lot of small adjustments to the seat support systems. More attention to these details has evolved into comfort and safety of the driver. What is this Trend now in Seating Systems? In […]
igus and its iglidur range of motion plastic products are the world’s largest manufacturer of polymer plain bearings. In the blogs previous sessions, you saw how igus’s performance polymers are built and the trade name of this range of products as iglidur. With our years of research, constant blending of different components inside iglidur (Base […]
Automotive companies face many challenges in their production lines like testing, inspection, precision and so on. We came across one such situation where an automobile engine manufacturer was facing a problem in their engine valve inspection line. The problem was that each of the valve guide pins should be positioned precisely to get the exact […]
The materials with which igus e-chains are made have to go under a great deal of stress such as pressure and tensile strain, and they are made to be abrasion-resistant, very sturdy and have a high modulus of elasticity, whereby they must also exhibit stable behaviour at high and low temperatures and be resistant to […]