igus:bike World Tour

Shery George | 21 November 2024

igus® was founded on October 15, 1964, in a garage in Cologne-Mülheim. Since then, we’ve been creating innovative, lubrication-free plastics that keep the world moving. Our products are used in cars, cranes, furniture, machines, robots, and even bicycles. One example is the igus®, a unique urban bike made from recycled plastic. It showcases many of […]

Read more...

Cables in Radioactive Environments

Shery George | 12 June 2024

Our chainflex cables are versatile and can be used in many different applications. They work well indoors and outdoors, in hot and cold places, in cleanrooms, and in oily air. But how do these cables perform as cables in radioactive environments? What is Radiation? Radiation is the movement of particles or waves. They are subdivided […]

Read more...

Why should you chooseplastic insert bearings overmetal?

Shery George | 28 May 2024

Anyone who’s worked with metallic insert bearings is likely aware of the frequent — and frankly tedious — relubrication efforts required for such components. Without the proper lubrication, these bearings are almost certain to wear prematurely and fail, leading to costly downtime and lost production. This may seem like an unavoidable reality, however there’s a […]

Read more...

What is igubal and what benefits do they offer in the Automotive Industry?

Shery George | 17 August 2022

Several industrial applications require bearings with self-aligning features and this is generally achieved by using spherical bearings. A spherical plain bearing is a bearing that permits angular movement around a central point. igubal is a range of polymer spherical bearings from igus GmbH. Like all the other products from igus, igubal bearings offer many advantages over metal spherical bearings. Here are […]

Read more...

Latest news

Hard or soft cable for e- chains: which is best?

Shery George | 28 March 2023

No matter whether you call it energy chain, e-chain or a drag chain, it also does not matter whether cables have Flexible Dynamic (FD), highly flexible (HF) or “chain” in the name. It is not the name that matters, but rather the function and durability. So, which is best? A “hard” or a “soft” cable […]

Read more...

Next Gen Connector – modular connector used for?

Shery George | 28 March 2023

The igus module connect has been developed as the next level of plug-and-play solutions. It features highly flexible housing that offers multiple inserts covering power, signal, data and pneumatic connections in one module. But what are modular connectors used for? Tell me more! What are modular connector used for? Vote Up +0 Vote Down -0You […]

Read more...

Machined bearing prototypes for new developments or tests

Shery George | 6 March 2023

When a new product is being developed for food, packaging, or beverage machine test phase, receiving prototype samples of a plain bearing or other machined components as quickly as possible is very important. iglidur polymer bar stock allows such components to be manufactured easily … with no minimum order quantity. It is available as plates, […]

Read more...

Maintenance-free knife edge rollers for the food & packaging industry

Shery George | 20 October 2022

Knife edge rollers are designed to reduce the gaps and ensure safe transfer of small parts from one conveyor belt to another. Especially in the food & packaging industry, during transfer of small food products like cookies, cakes, biscuits, pasta products, they may slide into the gap between the two conveyor belts if there is a […]

Read more...