Industry
When a new product is being developed for food, packaging, or beverage machine test phase, receiving prototype samples of a plain bearing or other machined components as quickly as possible is very important. iglidur polymer bar stock allows such components to be manufactured easily … with no minimum order quantity. It is available as plates, […]
Knife edge rollers are designed to reduce the gaps and ensure safe transfer of small parts from one conveyor belt to another. Especially in the food & packaging industry, during transfer of small food products like cookies, cakes, biscuits, pasta products, they may slide into the gap between the two conveyor belts if there is a […]
Ached Backs and Strained necks are not a good combination for a long drive. A good comfortable driving position is derived from a lot of small adjustments to the seat support systems. More attention to these details has evolved into comfort and safety of the driver. What is this Trend now in Seating Systems? In […]
igus and its iglidur range of motion plastic products are the world’s largest manufacturer of polymer plain bearings. In the blogs previous sessions, you saw how igus’s performance polymers are built and the trade name of this range of products as iglidur. With our years of research, constant blending of different components inside iglidur (Base […]
The materials with which igus e-chains are made have to go under a great deal of stress such as pressure and tensile strain, and they are made to be abrasion-resistant, very sturdy and have a high modulus of elasticity, whereby they must also exhibit stable behaviour at high and low temperatures and be resistant to […]
The interior separation is an important component of energy chains and serves to separate or subdivide different media within the guide. Because the service life of the system can only be increased with the correct arrangement of the cables. In this article, you will learn more about the different components of interior separation and how you can find the […]
System E6 offers many advantages besides its long service life. It features extremely quiet, low-vibration operation, complementing the low-vibration linear drive concept in high-speed & low noise machine tool applications. It minimizes the polygon effect which can occur during the rolling motion of an e-chain®. The ultra-low noise levels have been confirmed in a recent report […]
P4HD.56.R: suitable for long travels, high speeds, heavy cable loads and Industry 4.0 Container cranes in ports around the world will be even more powerful and fail-safe in the future. This is due to the fact that igus is launching P4HD.56.R – a new heavy-duty energy chain prepared for long travels, high speeds, heavy cable […]
Several industrial applications require bearings with self-aligning features and this is generally achieved by using spherical bearings. A spherical plain bearing is a bearing that permits angular movement around a central point. igubal is a range of polymer spherical bearings from igus GmbH. Like all the other products from igus, igubal bearings offer many advantages over metal spherical bearings. Here are […]
“You don’t have to reinvent a wheel, just realign it.” This old quote holds true for a modern-day design engineer designing a machine. It is the reason why the designer likes to use off the shelf, standard “bought-out” parts wherever possible in his design. Fortunately, in today’s industry most of the established company has a […]