If you are facing scoring mark issue in your existing stainless steel linear guide solution then you are reading a right article. People are using SS linear guide solution mostly in pharmaceutical, packaging & chemical industry where highly corrosive substances are coming in directly contact with system. Stainless steel corrosion resistance is a result of […]
In general, efficiency indicates how high the effectiveness of a device is when conversion losses are taken into account. The efficiency describes the relation between the delivered power (effective output) and the supplied power or loss and expenditure. In the calculation, the efficiency is abbreviated with a small eta (η). The result of the efficiency […]
Whether in dosing systems, on conveyor belts of filling systems or in labelling technology: you will find sheet metal and parts that are exposed to friction and wear in all these places. To increase the service life of the metallic components, igus has developed new coating material IC-05 which is compliant with FDA as well as […]
Automation of the manufacturing process is a critical need for the current industry to stay competitive and improve quality and reliability. This also allows better use of human resources. With the pandemic and shortage for manpower in the current scenario we are also pushed by circumstances. Most of the repetitive, mundane tasks could be automated. […]
Igus has introduced Stepper & DC Drives for controlling DC, BLDC & stepper motors. This article is particularly about the Stepper Drive, which is called igus D1 Drive. We offer this D1 (Stepper Drive) along with our screw-driven and belt-driven systems. The igus D1 Drive acts as a versatile single-axis motor controller, ensuring smooth stepper […]
igus has introduced 7th axis for Robots which is one on the NEWS product on 2020. The idea behind this development is that the existing robots can be moved up to 3 meters either in Vertical or Horizontal orientation – so one robot can handle two or three machines depending on the space available. Construction: […]
For applications that require vertical cable management, especially those with space constraints, the zigzag energy e-chain modules from igus® have proven to be particularly successful. Standard zigzag energy chain modules are available from igus®, offering a space-saving and cost-effective solution for applications requiring vertically moving cable management. Ideal for stage technology, cranes, telescopic antennae etc, this innovative solution was previously only available […]
Energy chains are often called by other names, such as drag chains and cable carriers. Fundamentally this is what they are. These chain systems are designed to guide and protect cables and hoses carrying energy, data and liquid safely. The goal is to ensure an uninterrupted supply. Many moving parts within a machine need to have a power source supplied […]
Anti-static component properties along with lubrication free, suitability for intensive cleaning agents , hygienic design & long service life are indispensable in packaging technology. The different packaging machines like thermoforming machines , Form,fill & seal machines , labelling machines, blister packaging machine , uses rollers for film deflection and may face some of the below […]
Especially now, preventive hygiene measures, or hygiene management, are in the spotlight. Especially in public facilities such as hotels, schools or hospitals, they play an indispensable role. Disinfection robots can provide a remedy here. But how safe is this new technology and is the use of robots worthwhile for public institutions? Time to take a […]