igus® was founded on October 15, 1964, in a garage in Cologne-Mülheim. Since then, we’ve been creating innovative, lubrication-free plastics that keep the world moving. Our products are used in cars, cranes, furniture, machines, robots, and even bicycles. One example is the igus®, a unique urban bike made from recycled plastic. It showcases many of […]
Our chainflex cables are versatile and can be used in many different applications. They work well indoors and outdoors, in hot and cold places, in cleanrooms, and in oily air. But how do these cables perform as cables in radioactive environments? What is Radiation? Radiation is the movement of particles or waves. They are subdivided […]
Anyone who’s worked with metallic insert bearings is likely aware of the frequent — and frankly tedious — relubrication efforts required for such components. Without the proper lubrication, these bearings are almost certain to wear prematurely and fail, leading to costly downtime and lost production. This may seem like an unavoidable reality, however there’s a […]
Several industrial applications require bearings with self-aligning features and this is generally achieved by using spherical bearings. A spherical plain bearing is a bearing that permits angular movement around a central point. igubal is a range of polymer spherical bearings from igus GmbH. Like all the other products from igus, igubal bearings offer many advantages over metal spherical bearings. Here are […]
Plain bearings stand out from ball or rolling bearings due to their less complicated design. But is this simplicity always true? The reality is, that various types of plain bearings have distinct constructions and workings. In this blog, we’ll explore the structure of the most common plain bearings. Overview of plain bearings and how they […]
Applications for the ninth vector award are now being accepted/deadline: 9th February 2024 Calling engineers from all over the world: the igus vector award is entering its next round. For the ninth time, igus is honouring design engineers and project managers for creative, courageous use of energy supply systems and cables made of high-performance plastic. […]
drylin econ entry-level series for simple adjustment and positioning tasks reduces costs by around 80% Injection-moulded from regranulated high-performance plastic and therefore very cost-effective and sustainable, the new polymer carriages from the igus drylin econ series make adjustment and positioning tasks simple. They cost less than 20% of what their milled aluminium counterparts do. Thanks […]
The world is becoming increasingly interconnected. Everything has to be available at all times. AI and chatbots are taking on more and more tasks. But past problems have shown us that supply chains can be disrupted and major problems can arise. That’s why we have set up a global network of production and storage locations […]