Industry
Anti-static component properties along with lubrication free, suitability for intensive cleaning agents , hygienic design & long service life are indispensable in packaging technology. The different packaging machines like thermoforming machines , Form,fill & seal machines , labelling machines, blister packaging machine , uses rollers for film deflection and may face some of the below […]
A gliding application frequently looks better than unsupported energy chain. This is not just because the straight line of the upper run, but also because the sag leading to the chain drop is eliminated compared to unsupported application. Unsupported systems will be better to use the space at the end of the travel (lesser Parking […]
You need a metallic component. You can quickly import the software model and the part comes out of the 3D printer in no time at all. Swarf doesn’t occur. There is practically no waste. This quickly leads to the question: can 3D printers replace classic machine tools? This blog examines this question for three relevant […]
Lathes, spindles and machine tools nearly always involve some form of rotation. The guidance of electric cables and hydraulic and pneumatic hoses is usually a difficult challenge. Even though an individual solution is needed for each machine, igus can offer Six varieties of Optimal Solution as below: Coiling of e-chain Coiling of e-chain with reverse […]
Wherever High precision range is required in the machine tool, plain bearings made of plastic reach their limits. However, in places where this is not the case, they can reduce costs and minimize maintenance. A typical place where our plain bearings show their full strength is in chain magazines of tool changing systems. The main […]
The Meat processing industry and it machines e.g steaks , fillets or sausages processing machines need to be tough and easy to clean. In this machines to fight germs the most aggressive cleaners and lots of water is use. As the application environments are critical the machine components like bearings will function in long run […]
The component service life plays an important role in the packaging and beverage industries, as the machines operate at high frequencies. During transportation activity ,there are various options for reductions of scratch marks and even damage. The service life of a glass beverage bottle is limited by the degree of damage to its exterior. Since […]
When its comes to guiding function of an energy chains , we need to ensure a design which is as open as possible and therefore easy to clean, or using materials that may be used in direct contact with food. We incorporated all these requirements into the development and implemented them with the TH3. Also […]
What are dancing rollers- Rollers which are used to feed the labels or films to machines & maintain specified tension to the film is known dancing rollers as they move freely up & down along with the film. What are […]
Different types of shafts are used in packaging , food and beverage industry based on their suitability for the particular application area. For e.g Stainless steel shafts are widely used as they are corrosion resistant , where the application works in moist environment or aggressive cleaning with chemicals is required . Steel shafts […]