Light & Quick Readychain Systems for Single Girder E.O.T. Cranes

Shery George | 8 December 2021

In modern crane technology Single Girder EOT Cranes are extensively used in warehouses, workshops, pre-cast manufacturing, sheet metal industry, automotive industries etc. Subsequently we also find applications in explosive, combustible, and corrosive environments as well. While majority of the single girder cranes fall into low duty cycles as the lifting capacities are also on the […]

Read more...

Maintenance free high performance igus polymer bearings for the pharmaceutical packaging industry

Shery George | 22 November 2021

With the changing times, the Indian Pharma industry is witnessing  dynamic changes & are adopting advanced technologies for their machines , manufacturing processes , packaging techniques and other related aspects , so  as to achieve greater output  & higher productivity without any compromise on the strict hygiene standards & to maintain the safety of the […]

Read more...

What are plain bearings and what advantages igus offers in Automotive industry?

Shery George | 12 November 2021

Plain bearings or commonly known as “bush”, bush bearing”, “bushing”, slide bearing” etc. are a much older technology when compared with ball bearings. Humans have been using plain bearings since year 3000BC. These are the simplest form of bearings without any rolling elements. Some of the most desired features of a plain bearings are – […]

Read more...

Selection of the Suitable mounting bracket

Shery George | 19 October 2021

Almost all mounting brackets are available in two variants. The first pivoting, the second is locking. At this point, many design engineers wonder when they should use the pivoting and when the locking version. Pivoting Type  Locking Type Pivoting mounting brackets are standard for gliding and horizontally unsupported applications: But why is that? The pivoting […]

Read more...

Distribution Rules for Hydraulic hoses in the energy chain

Shery George | 19 October 2021

Machine tools very often have hydraulic hoses that are guided in e-chains – for clamping devices, coolant circuits and other applications. For hoses, as for electrical cables, there are several items to consider in the design and fitting of energy chains. Rule 1 : Whether Crossbars every link or every second link ? If a […]

Read more...