Igus liner technology

igus introduces Stepper/DC drives.

Vishaka Upreti | 17 June 2021

igus has introduced Stepper motors and DC drives for controlling DC, BLDC motors, and stepper Motors. This article is particularly about the D1 Stepper Drive. We offer this D1 Stepper Drive along with our screw-driven systems and belt-driven systems. The drive is compatible with industrial controllers like Siemens and Beckhoff, as well as open-source modules […]

Read more...

igus polymer spherical bearings

How polymer spherical bearings ensure more efficient energy generation

Vishaka Upreti | 17 June 2021

Everyone has seen them at some point. Individual solar modules on a house roof or many of them arranged to create a solar power plant. These solar modules are generally fixed in place, oriented optimally to catch the sun. In large solar power plants, energy is generated more efficiently with special tracking systems, the “solar […]

Read more...

igubal bearings

igus® internal tests confirm the reliability of products for the solar industry

Vishaka Upreti | 17 June 2021

Producing energy from renewable sources is always associated with high costs and investments. Various factors such as procurement, financing, and operating costs play a significant role. An important consideration is the system’s service life – a long one means that these costs can be recouped over a longer period. Photovoltaic systems, especially solar modules, nowadays […]

Read more...

igus Lead screw

Polymer lead screw nuts and the influence of temperature

Vishaka Upreti | 8 June 2021

Lead screw drives are used in machines in a wide variety of industries. The demands on the lead screw drives therefore differ: high and low speeds and loads as well as wide temperature ranges or a continuous temperature of around 200°C. Even in these situations, lead screw nuts and lead screws have to work reliably. […]

Read more...

igus drylin

Reduce costs in vending machine construction with reliable components

Vishaka Upreti | 8 June 2021

How Reliable Vending Machine Components Help Reduce Costs Whether the snack dispenser in an office, the reverse vending machine in a shop or an ATM on the street, they all have to perform their service without interruption, if possible 24/7. This alone is a great challenge for a vending machine manufacturer, as customers do not […]

Read more...

igus e-chains

Are igus energy chains halogen-free?

Vishaka Upreti | 2 June 2021

Often the question is asked, whether igus e-chains contain chlorine? For someone who is not familiar with the subject, this question seems rather strange as mostly we associate chlorine with water purification in swimming pools. Therefore, let us go deeper into the subject. Classification of the elements Chlorine (Cl) belongs to the group of halogens (ancient Greek […]

Read more...

igus self aligning bearings

What is igubal and what benefits do they offer?

Vishaka Upreti | 24 May 2021

Many industrial applications need bearings with self-aligning features and this is generally achieved by using spherical bearings. A spherical plain bearing is a bearing that permits angular movement around a central point. igubal is range of polymer spherical bearings from igus GmbH. Like all other products from igus, igubal bearings offer many advantages against metal spherical bearings. Here are […]

Read more...

igus e-chains system

World record with 670 m! Longest travel installed with igus e-chains system.

Vishaka Upreti | 13 May 2021

igus India won the order for 2 x 670 m travel in a thermal power plant. igus believes that special solutions, be it conversion or new installation, do not need to be expensive. With over 20 years of experience in project work and more than 1,000 projects each year, igus has a rich modular system […]

Read more...

What is the CF8xx series all about?

Vishaka Upreti | 10 May 2021

The CF8xx series is part of the igus cable product portfolio. But what exactly is it all about? When can I use CF8xx products, and what is so special about the cables? What is the CF8xx series? The CF8xx series (CF880, 881, 890, 891, 888, 898, etc.) was launched a few years ago under the name […]

Read more...

The difference between a servo cable and a motor cable?

Vishaka Upreti | 10 May 2021

Electrical engineering is often concerned with motor cables as well as servo cables. But what is exactly the difference between a servo cable and a motor cable? And can I use a servo cable to connect a normal three-phase motor? What exactly are the differences? The fact is that both cables are designed to supply a motor with […]

Read more...