New low-cost igus carriage for curved rail made of recycled high-performance plastic

Shery George | 23 November 2023

drylin econ entry-level series for simple adjustment and positioning tasks reduces costs by around 80% Injection-moulded from regranulated high-performance plastic and therefore very cost-effective and sustainable, the new polymer carriages from the igus drylin econ series make adjustment and positioning tasks simple. They cost less than 20% of what their milled aluminium counterparts do. Thanks […]

Read more...

What does global, digital, and 24/7 mean for chainflex®?

Shery George | 25 October 2023

The world is becoming increasingly interconnected. Everything has to be available at all times. AI and chatbots are taking on more and more tasks. But past problems have shown us that supply chains can be disrupted and major problems can arise. That’s why we have set up a global network of production and storage locations […]

Read more...

The chainflex® service oasis

Shery George | 23 October 2023

In today’s increasingly globalised world, service is often a nuisance for everyone. You have a problem with a household appliance, perhaps an oven, and you have specifically chosen a German brand. Luckily, the instructions also include a flyer with service numbers for each country. But when you enter the number into your phone, you always […]

Read more...

Why Are Plastic Components Ideal for the Packaging and Food Industries?

Shery George | 1 August 2023

Bearings are on just about every machine imaginable in the packaging industry: tray sealing, dosing, cartooning, form fill and seal, tubular bagging, and sleeving and wrapping applications, just to name a few. So it is easy to see how machine builders and designers, whether for general packaging or the food and beverage industry, could bite-off more than […]

Read more...

Spherical bearings for weigher flaps

Shery George | 19 May 2023

igubal spherical bearings are self-aligning bearing elements manufactured completely from polymer and are therefore very lightweight. They are perfect for use in weighing systems. Individual scales, but also multihead weighers, can be found in various types of packaging machines (such as bag forming, filling and sealing machines). Because the products to be weighed and packaged […]

Read more...

7 Tips for selecting the optimum conveyor rollers

Shery George | 27 April 2023

The following blog provides tips for selecting the right guide roller for each application.  Tip 1: Determine the load profile-  At the beginning of each selection process, the conveyor system design engineer should determine the requirements for the drive rollers and guide rollers. They will often notice that they can use more cost-effective guide rollers […]

Read more...

Hard or soft cable for e- chains: which is best?

Shery George | 28 March 2023

No matter whether you call it energy chain, e-chain or a drag chain, it also does not matter whether cables have Flexible Dynamic (FD), highly flexible (HF) or “chain” in the name. It is not the name that matters, but rather the function and durability. So, which is best? A “hard” or a “soft” cable […]

Read more...

Next Gen Connector – modular connector used for?

Shery George | 28 March 2023

The igus module connect has been developed as the next level of plug-and-play solutions. It features highly flexible housing that offers multiple inserts covering power, signal, data and pneumatic connections in one module. But what are modular connectors used for? Tell me more! What are modular connector used for? Vote Up +0 Vote Down -0You […]

Read more...

Machined bearing prototypes for new developments or tests

Shery George | 6 March 2023

When a new product is being developed for food, packaging, or beverage machine test phase, receiving prototype samples of a plain bearing or other machined components as quickly as possible is very important. iglidur polymer bar stock allows such components to be manufactured easily … with no minimum order quantity. It is available as plates, […]

Read more...

Maintenance-free knife edge rollers for the food & packaging industry

Shery George | 20 October 2022

Knife edge rollers are designed to reduce the gaps and ensure safe transfer of small parts from one conveyor belt to another. Especially in the food & packaging industry, during transfer of small food products like cookies, cakes, biscuits, pasta products, they may slide into the gap between the two conveyor belts if there is a […]

Read more...