Industry
Anyone who’s worked with metallic insert bearings is likely aware of the frequent — and frankly tedious — relubrication efforts required for such components. Without the proper lubrication, these bearings are almost certain to wear prematurely and fail, leading to costly downtime and lost production. This may seem like an unavoidable reality, however there’s a […]
Bearings are on just about every machine imaginable in the packaging industry: tray sealing, dosing, cartooning, form fill and seal, tubular bagging, and sleeving and wrapping applications, just to name a few. So it is easy to see how machine builders and designers, whether for general packaging or the food and beverage industry, could bite-off more than […]
igubal spherical bearings are self-aligning bearing elements manufactured completely from polymer and are therefore very lightweight. They are perfect for use in weighing systems. Individual scales, but also multihead weighers, can be found in various types of packaging machines (such as bag forming, filling and sealing machines). Because the products to be weighed and packaged […]
The following blog provides tips for selecting the right guide roller for each application. Tip 1: Determine the load profile- At the beginning of each selection process, the conveyor system design engineer should determine the requirements for the drive rollers and guide rollers. They will often notice that they can use more cost-effective guide rollers […]
No matter whether you call it energy chain, e-chain or a drag chain, it also does not matter whether cables have Flexible Dynamic (FD), highly flexible (HF) or “chain” in the name. It is not the name that matters, but rather the function and durability. So, which is best? A “hard” or a “soft” cable […]
The igus module connect has been developed as the next level of plug-and-play solutions. It features highly flexible housing that offers multiple inserts covering power, signal, data and pneumatic connections in one module. But what are modular connectors used for? Tell me more! What are modular connector used for? Vote Up +0 Vote Down -0You […]
When a new product is being developed for food, packaging, or beverage machine test phase, receiving prototype samples of a plain bearing or other machined components as quickly as possible is very important. iglidur polymer bar stock allows such components to be manufactured easily … with no minimum order quantity. It is available as plates, […]
Knife edge rollers are designed to reduce the gaps and ensure safe transfer of small parts from one conveyor belt to another. Especially in the food & packaging industry, during transfer of small food products like cookies, cakes, biscuits, pasta products, they may slide into the gap between the two conveyor belts if there is a […]
Ached Backs and Strained necks are not a good combination for a long drive. A good comfortable driving position is derived from a lot of small adjustments to the seat support systems. More attention to these details has evolved into comfort and safety of the driver. What is this Trend now in Seating Systems? In […]
igus and its iglidur range of motion plastic products are the world’s largest manufacturer of polymer plain bearings. In the blogs previous sessions, you saw how igus’s performance polymers are built and the trade name of this range of products as iglidur. With our years of research, constant blending of different components inside iglidur (Base […]