My iglidur plain bearing breaks when it is being installed. What should I do?

Vishaka Upreti | 13 April 2021

< All Topics
Print

For uncomplicated and easy installation of our plain bearings, we recommend

–    a burr-free clean housing hole, ideally with slight chamfering

–    the hole tolerance H7

–    ensuring that the plain bearing is not more than 2 % larger than the hole before it is press-fitted

–    installation by means of a flat press without a centring or calibrating pin

You already voted!
Tags:
Previous Is the colour of the bearing freely selectable?
Next My iglidur plain bearing has become jammed on the shaft. What to do?

Related questions

You are also welcome to comment on the article - we look forward to your opinion!

Article keywords:

iglidur

Newsletter:

Choose a topic now