Do I need to axially secure the plain bearings?

Vishaka Upreti | 13 April 2021

< All Topics
Print

iglidur plain bearings are generally press fitted in the smaller housing hole. Certain parameters such as high or especially low temperatures, however, can diminish the press-fit – at least temporarily. In this case, technical measures are recommended, such as using collar bushings, other types of component or a more suitable iglidur material with a lower coefficient of thermal expansion.

You already voted!
Tags:
Previous Can I use iglidur plain bearings for heavy loads?
Next Do plain bearings comply with ESD or ATEX requirements?

Related questions

You are also welcome to comment on the article - we look forward to your opinion!

Article keywords:

iglidur

Newsletter:

Choose a topic now