The good thing about drylin® is that it’s not limited by speed – because we have no moving parts – these are gliding, sliding parts – nothing has to catch up with itself. The fastest application that I’ve worked with is actually in the textile industry – on looms, where they are carrying just a little, weaving threads. Now, they are travelling at 15m/s and the good thing is that it’s going very quickly, and most importantly the return is very quick as well. So, because it has no moving parts, it has nothing needing to stop, rotate and return on itself – and it can, therefore, work at very high speeds. These high speeds tend to be light loads, but these can, theoretically, even exceed 15m/s.