e-chain
igus India won the order for 2 x 670 m travel in a thermal power plant. igus believes that special solutions, be it conversion or new installation, do not need to be expensive. With over 20 years of experience in project work and more than 1,000 projects each year, igus has a rich modular system […]
The performance and reliability of a crane is directly dependent on how power reaches the system. There are various power supply options available and each option has certain parameters and requirements to be considered. This can mean that selecting the best type of system to implement can be complicated. Here we look at 2 possible options; Busbar […]
Mechanical engineers have to adapt their machines time and time again to a new situation. Customer requirements, quality assurance specifications, and even market needs are changing constantly. This also requires an adaptability of manufacturing companies and their plant – on the one hand to meet the existing demand and on the other hand to remain […]
The term e-chain is closely related to the terms drag chain, energy chain and energy supply system or energy guiding chain or even cable guidance systems. The e-chain describes a product that safely carries cables or even hoses, over a certain distance. They ensure the dependable supply of energy, data and signals while in constant motion. They […]