Can reduction of scratches on products during conveying is possible in Packaging & Beverage industries ?
Shery George | 2 September 2021
The component service life plays an important role in the packaging and beverage industries, as the machines operate at high frequencies. During transportation activity ,there are various options for reductions of scratch marks and even damage. The service life of a glass beverage bottle is limited by the degree of damage to its exterior.
Since many bottles are transported through various lanes at high speed from time to time , there is a possibility that they bump & strike against the lateral lanes made of stainless steel sheets with great force. This impact, as well as the friction of sliding past the lanes, wears the bottles’ exterior and might even damage it. The same problem occurs if the conveying surface is uneven.

Even in case of packed carton , the case is similar. The possibility of easily damage to aesthetics is more as they are more sensitive.

What easy options are there for protecting products?
Tribo Tape is the self lubricating & maintenance free polymer liner which is characterized by low coefficient of friction & low wear. When fixed on lateral lanes it provides slightly damping property and smooth surface which protects & prevents the products from damage or wear and hence results in longer service life . This allows glass bottles to be used many more times than they could be without additional protection.
https://www.igus.in/tribo-tape/sliding-tape
How can the tribo tape can be installed?

There are two options. One is to clamp or screw in the film. This depends on the contour and the support surface. The other is to simply use adhesive. The film is available with or without a self-adhesive back. The self-adhesive back must be removed from the protective film and, once the support surface has been thoroughly cleaned, the tribo tape can be easily fixed in place. This also makes replacing the tape easy if it becomes worn.
For more details of tribo tape , pls. go through below link.